Hard scale build up on exterior of copper pipe in plumbing system.


This temperature and pressure relief valve has become clogged with the accumulation of hard scale, which can lead to potentially dangerous conditions.


While effective in eliminating scale, water softeners come with a number of environmental drawbacks.


Chemical injection systems often fail in hot water systems and have high monthly costs.

The Scale Problem

What is Scale?

Many building owners and maintenance personnel are all too familiar with the troubles of scale. But, just what is it? Scale is an incrustation of calcium carbonate (CaCO3) that forms on imperfections on heating elements or within plumbing systems. It is primarily composed of calcium (Ca2+), magnesium (Mg2+) and bicarbonate (HCO3). Scale deposits grow over time and are highly insoluble, making scale extremely difficult to remove once formed and often leading to costly remediation efforts.

Why is Scale Harmful?

There are a number of issues associated with the growth of scale. First, as scale forms over time, it reduces the inner diameter of pipes and elbows, ultimately leading to restrictions in flow rate and pressure loss problems in systems. Second, scale often becomes encrusted on internal moving parts of valves & components, affecting their intended purpose or worse, causing safety failures. Lastly, in a boiler or hot water tank, heating elements can become coated with scale, reducing system efficiency and increasing operating costs for end users.

Scale Control Technologies

Water Softeners

Before OneFlow™, the most common approach to dealing with scale was the installation of a water softener. The never-ending consumable cost of salt, required for system regeneration, is expensive and must be considered in the overall cost equation. Although effective in dealing with most scale, water softeners come with some significant drawbacks including:

  • Harmful chloride discharge that negatively impacts the environment
  • The removal of beneficial minerals (calcium & magnesium) from drinking water
  • A backwashing and regeneration process that wastes water
  • Large floor space requirements for operation and storage of salt bags

Scale Inhibitors or Sequestrates

Scale sequestering systems introduce phosphate-based chemicals to inhibit scale. These systems work better in cold water applications but have a tendency to break down or fail in hot water. Similar to softeners, scale sequestering systems require the constant introduction of a chemical resulting in ongoing monthly costs to end users.

Magnets and Other Devices

Magnets, electro-magnets, radio frequency devices, electrical current systems and other "black magic" inventions have failed to pass any scale control standards designed by internationally recognized 3rd party testing agencies. While the manufacturers of these products may have in-house data to support their amazing scale control claims, none of these products have ever passed any international protocol for scale prevention. "Buyer Beware" is the best advice one can take if considering this gadgetry.

The Catalyst for Change

OneFlow™

Now there’s OneFlow™, the first physical water treatment technology to effectively control scale. OneFlow™ achieved a 99.6% effectiveness rating in scale prevention from DVGW (German Technical and Scientific Association for Gas and Water). Further, OneFlow’s media has been tested and certified for material safety to NSF/ANSI standard 42 & 61.

Learn more about OneFlow™