What's New - Check out our latest featured products and more!

FloodSafe® Connectors

Watts is pleased to introduce its new line of FloodSafe® Auto-Shutoff Connectors. The floodSafe's patented design protects against catastrophic water damage caused by burst, broken or ruptured water supply hoses and fittings. FloodSafe® connectors include a standard braided stainless steel flexible hose and a FloodSafe® shutoff device located on the inlet.

Problem

In recent years, losses due to water and mold damage to residential and commercial buildings have been steadily on the rise. Water supply hoses are vulnerable to a number of potential problems. Over time, hoses can become brittle and burst. Poorly manufactured hoses can break under normal pressure conditions and hoses used in public venues are highly vulnerable totampering by vandals. All of these conditions can lead to a flood of problems for homeowners, property managers and maintenance personnel.

Solution

Watts FloodSafe® auto-shutoff connectors protect against catastrophic water damage by automatically shutting off the water supply to plumbing fixtures/appliances if excess water flow is sensed. Water flow through the FloodSafe® device is limited to a factory preset flow rate, any flow over the preset rate will automatically shutoff all flow of water through the device.

How it Works

FloodSafe® is actuated by flow of cold or hot water in excess of the design flow rate indicated on the label. Once a downstream flow of water in excess of the flow required by any standard fixture/appliance is detected, FloodSafe® assumes a burst and the flow of water is shutoff. FloodSafe® remains in the closed position until it is reset. To help illustrate this, check out our FloodSafe® Video in our Media Center for full details.

Click here for the Floodsafe Video

Installing FloodSafe®

Installing FloodSafe® connectors is easy. Simply follow the steps below:

To Install:

  1. Turn off water supply at shutoff valve.
  2. Remove old supply connector.
  3. Install the end connection with the FloodSafe® device at the shutoff valve. Install the other end of the connector to the faucet inlet. Caution: Hand tighten the nuts plus ¼" turn with a wrench. Do not overtighten.
  4. Slowly turn on water at the shutoff valve to full open position.
  5. Check for leaks.

Important: Removing the faucet aerator or flow restrictor may cause the FloodSafe® to activate shutting off flow to the faucet.

Resetting FloodSafe®

Resetting FloodSafe® connectors if water flow has been stopped is easy.

Before proceeding, check for damage or rupture to the hose. Do not reactivate if a leak is evident.

To reactivate flow of water to the fixture:

  1. Close the shutoff valve to shut the water supply to the FloodSafe® connector
  2. Disconnect the FloodSafe® at the shutoff valve. This will automatically reset the FloodSafe® device.
  3. Reconnect the FloodSafe® according to installation instructions and turn on water supply to full open position. Check for leaks.

Available Models

Floodsafe Auto Shutoff Connectors

  • The only economical and secure safeguard against catastrophic water damage available on the market
  • Patented design
  • No mechanical moving parts during normal operation, ensuring years of maintenance free operation
  • Does not require electricity, batteries or any other source of power
  • Maintenance free
  • CSA, NSF and IAPMO Listed
  • Installs between the stop valve and the Fixture or appliance with the FloodSafe® device located at the stop valve

  • Acts as a water conservation device, by shutting off the water to the faucet when the mandated low restrictor is removed
  • Available for faucets, toilets, ice makers, dishwashers and washing machines

More Information

Click here to download the FloodSafe® product brochure.

Get Adobe Acrobat

Please Note: Watts literature requires Adobe Acrobat Reader to view.

Additional Information

Danger – Scalding Lurks!
Every year, thousands of people suffer serious thermal shock or scalding injuries in their bathtubs, sinks and showers.

Click here for informative resources to help you protect against these dangers.

Learn About

Steam Traps
This guide to Steam Traps explains how each style of trap functions and how to select the proper steam trap for your application. Includes application diagrams and trap cutaway views.

To learn more about Steam Traps and how they work, click here.