Your Country
USA Flag Image
Watts
 
Skip Navigation

USC Cross-Connections Study
Introduction and Results
Toilet
Laundry Sink
Outdoor Faucet
Lawn Irrigation System
Heating/Cooling Systems
   
 
 
  Introduction and Results
 

The University of Southern California Foundation for Cross-Connection Control and Hydraulic Research (USC-FCCCHR) performed a study in late 2002 and early 2003 to determine the degree of protection against backflow that is present in today’s homes.

The results are summarized as follows:

  • 9.6% of the homes surveyed had direct health hazard cross-connections
  • 73% of the homes’ water uses were unprotected cross-connections
  • 95.7% of the homes had either a direct or indirect cross-connection to a health hazard
  • 91% of the homes had unprotected hose bibbs
  • 43.6% of the homes had heating/cooling system health hazard cross-connections

Watts reminds you to check the following common cross-connections in homes to ensure the
proper protection against backflow:

  Toilet
 
When water leaves the drinking water supply system and flows into the toilet tank, the water must be prevented from being drawn back into the water supply. The water in the toilet tank is often treated with cleansing chemicals that are not safe to drink.

An anti-siphon ballcock assembly should be installed in the toilet tank. This will protect against backsiphonage. The ball cock can also serve as a thermal expansion relief device, if equipped with an auxiliary relief valve. The relief valve should govern the preset pressure to 80psi or less.

Laundry Sink
 
To make the laundry sink safe, a hose bibb vacuum breaker is needed. This is a small, inexpensive device that simply attaches to the threaded end of the faucet as with the outside water faucets (sill cocks). It prevents contaminated water in the sink from being siphoned
back into the drinking water supply.

Outdoor Faucet

 

The ordinary garden hose is the most common way to contaminate the water supply. This can happen when one end of the hose is attached to an outdoor faucet (sill cock), and the other end is connected to an aspirator type bottle, insecticides or other chemicals in the aspirator
bottle can be siphoned back into the drinking water supply.

You can easily prevent the possibility of this type of contamination by installing a hose bibb vacuum breaker. This is a small, inexpensive device that simply attaches to a threaded water faucet.

Lawn Irrigation System

 
Lawn irrigation systems need a vacuum breaker backflow preventer to protect against lawn and pesticide chemicals being drawn in from the lawn and back into the drinking water supply.
Heating/Cooling Systems

 
A hot water system may be used to heat the home. You can ensure the protection of the safe drinking water system by making sure a dual check with atmospheric vent is installed. This will protect against stagnant or chemically treated water from recirculating back into the
water supply.
     
USC Cross-Connections in Household Plumbing Systems Study
There are a number of potential cross-connections in household plumbing systems that must be protected against backflow. To learn more about these hazards and to download a recent study from USC on cross-connections in household plumbing systems,

For more info, click here.
Stop Backflow News
Backflow contamination can have hazardous or even fatal results. It is essential that backflow prevention programs be put in place and maintained on an ongoing basis. Stop Backflow news presents many case histories outlining the effects of backflow contamination.

To download this brochure, click here.

Canadian Customers
Careers / Investors / Terms of Use / Privacy Policy
© 2009 Watts
A Watts Water Technologies Company. All Rights Reserved.