Thermostatic Mixing Valves
The Dangers of Hot Water
Every year, thousands of people in the U.S.A. suffer serious thermal shock
or scalding injuries in their bathtubs, sinks and showers. Additional untold
numbers become ill due to water-borne bacteria, such as Legionella.
Problem: Thermal Shock
Often, injuries in the shower are caused by slips and falls in reaction to a
sudden increase or decrease in water temperature. Ideally, if the supply of
cold or hot water is lost, the water flow should be shut down immediately.
Termination of flow would eliminate the instinctive but dangerous reaction
to move quickly away from a too hot or too cold water stream.
Solution:
Watts Thermostatic Mixing Valves maintain and limit mixed hot water to a
desired, selectable temperature, helping to minimize thermal shock.
| Problem: Scalding |
 |
More than 90% of scalding incidents occur in the home. The tender skin of very young children and the slow reaction time of the elderly and the handicapped make them most vulnerable to serious hot water burns.Scalding injuries are tremendously painful, and the effects can last for years. Scalding occurs for a variety of reasons. In some cases, water heater thermostats are faulty, or set too high. In others, temperature regulating valves at the domestic hot water source are either malfunctioning or missing altogether. Water heaters are normally set to temperatures above 131°F (55°C) to prevent development of harmful bacteria, such as Legionella, in the water supply. Water at temperatures above 106°F (41°C) are painful. At a temperature of 131°F (55°C), a child can be scalded in less than 4 seconds. |
Solution:
Watts Thermostatic Mixing Valves maintain and limit the mixed hot water to a desirable
selectable temperature, helping to prevent scalding injury.
| Problem: Legionella Bacteria |
| Legionella is the bacteria responsible for Legionnaire’s Disease, an acute bacterial infection of the lower respiratory tract. This bacterium was first identified in 1977 by the Centers for Disease Control as the cause of an outbreak of pneumonia that caused 34 deaths at a 1976 American Legion Convention in Philadelphia. Pontiac Fever is a less severe, non-pneumonia, flu-like disease that is associated with and likely caused by Legionella bacteria.
Legionella is a fairly common water bacteria and has been found to exist widely in many surface water sources such as; lakes, rivers, streams and ponds. It can also be found in ground water sources and some soils. At the levels found in these naturally occurring sources it typically does not pose a threat to public health. When the bacterium enters a domestic water system |
 |
it can find an ideal host environment of warm water temperatures (105-115°F), stagnant water areas (storage tanks and dead-end piping legs) and ample food sources (sediment, scale, deposits and biofilm). Under these conditions Legionella can rapidly colonize, forming higher concentrations that can pose the public health threat of Legionnaire’s Disease.
There are many methods of controlling colonization of Legionella bacteria. However, a widely accepted and preferred method is to maintain the hot water system storage temperature continually at or above 140°F. Unfortunately, the elevated temperature necessary to minimize the growth of and kill Legionella bacteria has the potential to cause serious thermal shock and scalding injuries. |
Solution:
Watts Thermostatic Mixing Valves maintain and limit the mixed hot water to a desirable,
selectable temperature allowing for the storage of domestic hot water at the higher
temperatures necessary to reduce the risk of Legionella growth in the system.
Many shower and combination tub/shower mixing valves in today’s homes use a
pressure balanced design. Unfortunately, pressure balanced type valves do not automatically
control outlet temperatures, nor do they automatically limit outlet temperatures
should the supply temperatures dramatically increase or decrease. Such limitations are
potentially dangerous. Further, to prevent users from adjusting the valve beyond a safe
operating temperature, pressure balanced valves require setting of the limit stop by the
installer. In addition, to accommodate future changes in the hot or cold water temperature,
the limit stop would need to be re-set.
By contrast, Watts Thermostatic Mixing Valves offer precise control of the outlet temperatures,
no matter how the supply temperatures or pressures vary over time.
| Since 1874 Watts has set the standard for the latest valve technology. Whether it is our pressure reducing valves to regulate steam or water, relief valves to ensure safe operation of water heaters or boilers or backflow prevention devices to help prevent cross-contamination of water supplies, Watts has earned a reputation for safety, reliability and innovation. |
 |
With widespread industry attention over the safe storage and distribution of domestic
hot water due to concerns of tap water scalding, thermal shock and Legionella, Watts
has again taken a leadership role by providing a complete line of thermostatic mixing
valves, which provide safe, accurate control of hot water from its source through to its
final use.
If you
have any questions or would like additional information on how to protect against the
dangers of scalding, thermal shock and Legionella growth, please visit our “Danger –
Scalding Lurks” page, or contact
your local authorized Watts Representative.
ASSE 1016 covers the delivery of water at the individual fixtures that are adjusted and
controlled by the user. Therefore, it addresses very precise and immediate temperature
regulation requirements. This standard covers three types of valves:
Pressure Balancing, Thermostatic and Combined Pressure
Balancing/Thermostatic. Watts ASSE 1016 listed valves meet the
thermostatic requirements of this standard.
ASSE 1070 is a recently approved standard and the newest of the three
standards. It covers control of maximum temperature to a fixture or group
of fixtures; such as sinks, lavatories or bathtubs. The device may either be the final
temperature regulation or have water further tempered downstream with the addition of
cold water.
ASSE 1017, on the other hand, does not address final temperature control at fixtures
and appliances. It is concerned with valves used at the source of hot water for distribution
to the supply system, and therefore allows wider variation of the outlet temperature
at higher flow rates.
ASSE 1017 listed devices should never be used to deliver water directly to the user.
These valves should be used in combination with an ASSE 1016 and/or
ASSE 1070
listed devices.
For more information, please check the ASSE website at:
www.ASSE-plumbing.org.
Upon use of tempered water, a thermostat in the mixing chamber of the valve senses
the outlet temperature. The thermostat automatically positions a seat assembly which
controls the flow of hot and cold water supplied to the mixing chamber. If the
mixed outlet temperature increases, the thermostat will expand moving the seat
assembly to allow the cold water inlet port to open more fully and at the same
time restricting the hot water inlet port. Conversely, if the mixed outlet temperature
decreases, the thermostat will contract moving the seat assembly to allow
the hot water inlet port to open more fully and at the same time restricting the
cold water inlet port. In both cases the mixed outlet water temperature is automatically
and continually maintained at the preset temperature within the tolerances
of the valve. In the event of a cold or hot water supply failure, the seat assembly
moves to an extreme position shutting off the hot or cold inlet water port. A mechanical adjustment permits selection of the desired outlet water temperature within range of
the valve.
Why They Are Used
Supply Systems
Mixing valves provide the following benefits:
- The water temperature that is discharged directly from a water heater can vary
±10°F or more. This can be due to tolerance of control devices, inlet water
temperature changes and stacking (higher water temperatures at the top of
the water heater). Use of a thermostatic mixing valve assures constant outlet
water temperature even with variations in hot or cold water supply temperature.**
- If a water heater is operated at lower temperatures, high flow demand situations
can result in a reduction of hot water supply temperatures if the recovery time of the
water heater is not sufficient for the flow demand. Using a hot water extender or
mixing valve allows the water heater to be operated at higher temperatures, extending
the effective system flow rate and preventing the growth of Legionella.
- To be able to supply peak demands for domestic hot water it is often necessary to
provide high capacity water heaters with high recovery rates. Use of a hot water
extender can reduce the size/BTU requirements needed to provide capacity for
peak system demands.
At the Fixture
Heat loss in the system piping can result in varying temperatures of the hot and cold
water supplied to fixtures. The use of thermostatic mixing valves assures constant safe
hot water temperature at the point of delivery to the fixture.
** Please refer to specification for the selected model to determine the allowable inlet
temperature range to maintain a desired outlet temperature.
Heat Traps
- All mixing valves used at the source of supply should be trapped. Trapping the valve
helps reduce mineral deposits and premature component wear.
- Heat traps help reduce convection loss also know as thermosiphoning, increasing
system efficiency.
Stop Valves
- All mixing valves should be installed with a means to isolate the valve for service
and repair.
Check Valves
- Check valves assure flow of water in one direction. They prevent thermal siphoning
of hot water to the cold water supply.
- The addition of check valves should be considered whenever the potential exists for
extreme differential pressures between the hot and cold water supply.
- Check valves are a requirement for compliance with ASSE Standard 1017 applications.
Watts Series USG, MMV and 1170 come standard with integral check valves.
Strainers
- Water supply systems should be thoroughly flushed prior to placing mixing valves
in service.
- Installation of additional strainers in the supply piping is recommended in systems
where water can contain particles that could impede the proper operation of the
mixing valve. Watts Series MMV and 1170 include inlet filters to provide protection
against supply line debris.
Maximum Pressure
This is the maximum pressure that the valve could be subjected to during normal
operation. Normal residential water system pressures should be limited to 80psi
(552 kPa) as required by national codes.
Maximum Temperature
This is the maximum temperature that the valve could be subjected to during normal
operation. Exceeding the maximum temperature could cause failure of internal components.
Minimum Flow
A minimum flow of water through the valve is required to provide accurate temperature
control. Water flow below the listed minimum could result in increased outlet deviations.
Minimum Inlet Differential
This is the minimum difference between the hot and cold temperature that is required
to produce the desired outlet temperature.
At the Fixture
Delivery of water to fixtures intended for use in bathing or washing should always be
controlled by valves listed to ASSE Standard 1016 Type T or ASSE Standard 1070
such as Watts Series MMV, L111 and USG mixing valves.
ASSE 1016 listed valves provide the user with both scald protection and thermal
shock protection. ASSE 1070 listed valves provide the user with scald protection only.
These valves should never be set to exceed a maximum temperature of
120°F (49°C). (Watts recommends the maximum temperature of 110°F
(43°C) for shower and bathing fixtures.)
Supply Systems
The control of water temperature for the source of supply should be
controlled by mixing valves such as ASSE 1017 listed Watts Series 1170,
L1170 and MMV.
These valves can also be used for re-circulation systems to maintain domestic hot
water supply temperatures at levels (temperatures above 131°F (55°C)) that prevent
the growth of harmful bacteria such as Legionella.
Radiant Heat Systems
Either a Watts 1170 or an L1170 mixing valve can be used for radiant heat systems.
However, it is important that a boiler’s high temperature limits do not exceed the maximum
temperature rating of the system components. This will protect against component
temperature failure should dirt, sediment or other mechanical failure cause a
mixing valve to become inoperable.
Periodic Inspection
Regular inspection of mixing valves is recommended to assure maximum valve life
and a properly functioning system. Corrosive water conditions, unauthorized adjustments
or repairs can be detected during inspection and service of the valve. The
frequency of cleaning depends upon local water conditions.
|
 |
 |
More Information
|
|
|
|
Watts Mixing Valves
Learn more about Watts’ newest mixing valves, Series 1170-M2 and MMV-M1 feature “Best in Class” flow rates and superior temperature control.
For more information, click here. |
|
 |
|
|
Danger – Scalding Lurks!
Every year, thousands of people in the United States suffer serious thermal shock or scalding injuries in their bathtubs, sinks and showers.
Click here for informative resources to help you protect against these dangers. |
|
|
|