Your Country
USA Flag Image
Watts
 
Skip Navigation

Water Pressure Reducing Valves

Water Pressure Reducing Valves
Promoting Water Conservation
What is a Water Pressure Reducing Valve?
How Does Watts Direct Acting Water Pressure Reducing Valve Work?
Sizing a Water Pressure Reducing Valve for Your Application
Choosing the Correct Installation Configuration
Two-Stage Serial Reduction Configuration
Parallel Installation
Water Pressure Reducing Valve Option Guide
End Connections
Using Performance Curves
Click here for a Printable Version
   
 
Water Pressure Reducing Valves

Ensuring Practical, Safe Working Water Pressures Municipal and private water supply companies use pumps and pumping stations to boost water supply pressures in supply mains to be able to supply water for fire fighting, high rise buildings to overcome loss of pressure as the elevation increases, and to maintain water supply in water towers and supply tanks. Pressure in water supply mains can exceed 200psi. Most plumbing codes require water pressure reducing valves on domestic systems where the municipal water main’s pressure exceeds 80psi. Higher pressures could rupture pipes, damage fixtures,and injure the people using them.
 
   
 
Promoting Water Conservation

High water pressures waste water. Many municipalities today not only charge homeowners and businesses high rates for water consumption, but also charge consumers equally high rates for the disposal of wastewater. Furthermore, reducing water consumption, reduces the excess energy required for heating additional hot water.

Water Savings: Twice as much water flows through a system at 150psi pressure than at 50psi. Much of this additional water is wasted.

Energy Savings: If less water flows through the system, then less energy is needed to heat domestic hot water. Calculations show that a Watts water pressure reducing valve can save as much as 30% on domestic water heating costs.

Wastewater Savings: When the community’s wastewater treatment load is reduced, cost benefits accrue to both the environment and your bottom line. Many municipalities prorate sewer usage fees based upon the water meter reading.
 
 
What is a Water Pressure Reducing Valve?

There are two types of water pressure reducing valves, direct acting and pilot operated. Both use globe or angle style bodies. Valves used on smaller piping diameter units are cast from brass; larger piping diameter units are made from ductile iron. Direct acting valves, the more popular type of a water pressure reducing valves, consist of globe-type bodies with a spring-loaded, heat-resistant diaphragm connected to the outlet of the valve that acts upon a spring. This spring holds a pre-set tension on the valve seat installed with a pressure equalizing mechanism for precise water pressure control.
 
   
 
How Does Watts Direct Acting Water Pressure
Reducing Valve Work?

Installed in series directly after the water meter in homes, commercial buildings, and manufacturing plants, a water pressure reducing valve automatically reduces the pressure fromthe water supply main to alower, more sensible pressure.

Water entering the valve from municipal mains is constricted within the valve body and directed through the inner chamber controlled by an adjustable spring loaded diaphragm and disc. Even if the supply water pressure fluctuates, the pressure reducing valve ensures a constant flow of water at a functional pressure, as long as the supply pressure does not drop below the valve’s pre-set pressure.
 
   
 
Sizing a Water Pressure Reducing Valve
for Your Application

A properly sized valve prevents noisy operation or premature valve failure. Over sizing water pressure reducing valves can lead to problems such as wire draw under low flow conditions. In general, the minimum flow through a water pressure reducing valve should be 10% to 15% of the maximum flow rate desired in the system. Also, water pressure reducing valves should be selected based on the flow and pressure ranges listed in the literature, not the size of the pipe to which they will be attached. You should select a regulator whose operating pressures fall within the middle of its rated range.
 
   
 
Choosing the Correct Installation Configuration

Watts water pressure reducing valves can increase your water system’s performance, reduce operating costs, and ensure a longer life for other plumbing fixtures. Most simple pressure reducing applications require the installation of a single regulator. However, there are applications that require the use of more than one unit installed in a specific system configuration. When there is wide variation in pressure between the municipal main’s inflow pressure and the functional pressure needed within the building, or when the main’s pressure exceeds 200psi, you should consider using a two-stage, serial reduction configuration. When you want to maintain a continuous supply of water at reduced pressures, you should consider a parallel installation.
 
   
 
Two-Stage Serial Reduction Configuration

The two-stage serial reduction approach uses two valves in series to reduce or eliminate extreme variations between the water main’s inflow pressure and the desired, final reduced pressure. Two stage reduction is recommended when initial pressures are 200psi or greater, or when the desired pressure reduction ratio is greater than 4:1, e.g., from 200psi to
50psi, or where the inflow pressure fluctuates greatly. The advantage of two-stage serial reduction is that neither valve is subjected to extreme pressure differentials, thus prolonging valve life and delivering more precise pressure regulation.
 
   
 
Parallel Installation

The parallel installation makes use of two or more smaller size water pressure reducing valves serving a large size supply pipe main. This approach should be used wherever there is a wide variation of reduced pressure requirements such as an apartment building where demand could be .5 gpm at 1am and 100 gpm at 6am and
where you must maintain a continuous water supply. Parallel installations also offer the advantage of providing increased capacity where needed beyond that provided by a single valve. In addition, the parallel configuration improves valve performance for wide variable demands and permits servicing of an individual valve without shutting down water flow to the building completely, thus avoiding costly shutdowns.
 
   
 
Water Pressure Reducing Valve Option Guide

End connections

To facilitate installation and servicing of the regulator, Watts offers a variety of end fitting configurations, which include union fittings (female threaded, solder, cpvc, and pex), flanged valves, water meter threads and special lay lengths for water meter installations. Please refer to the valve model for specific availability of end connection options.
 
   
 
Using Performance Curves

To match the valve characteristics to system requirements Watts provides performance curves on WPRV specification sheets for each type and size of valve giving the capacities of each with reduced pressure fall-offs up to 25psi. By the use of these charts, the most suitable and economical valve can be selected to satisfy the job requirements. The charts or curves for all types are plotted on a simple basis of rate of flow plotted against the reduced pressure fall-off. In the left hand column, the reduced pressure fall-off is listed up to 25psi. Along the bottom, is listed capacity in terms of gallons per minute flow. In the reduced pressure fall-off column, the “0" represents the reduced pressure setting of the valve when there is no flow (reduced lock-up pressure). The example below illustrates how to use these performance curves.

Requires Adobe Flash Player to view.
Broadband connection recommended
 
   
 

Want more information?

For more information please see our
Watts Water Pressure Reducing Valves product guide.

Click here to get the product guide.

Acrobat Reader is needed to view.
Click Here to download Acrobat Reader.

 
     
Danger – Scalding Lurks!
Every year, thousands of people in the United States suffer serious thermal shock or scalding injuries in their bathtubs, sinks and showers.

Click here for informative resources to help you protect against these dangers.
This guide to Steam Traps explains how each style of trap functions and how to select the proper steam trap for your application. Includes application diagrams and trap cutaway views.

To learn more about Steam Traps and how they work, click here.

Canadian Customers
Careers / Investors / Terms of Use / Privacy Policy
© 2009 Watts
A Watts Water Technologies Company. All Rights Reserved.