Your Country
USA Flag Image
Watts
 
Skip Navigation

Potable Water Expansion Tank Sizing
 

TO PROPERLY SIZE A WATTS REGULATOR SERIES PLT, DET OR DETA POTABLE WATER EXPANSION TANK:

Enter the appropriate information in the boxes below..

* Required Fields
Water Heater * Gallons
Supply Pressure *
The set pressure of the water pressure reducing valve or maximum system pressure.
PSI
Air Pre-Charge *
40psi Air Charge is Standard. Never exceed 80psi Pre-Charge.
PSI
Relief Valve *
The set pressure of the T&P valve or the secondary relief valve setting.
PSI
Inital Temperature - Start *
NOTE: Set the cold water start temperature to 90°F. Lower start temperatures should only be used if the entire contents of the water heater are drained on each use.
°F
Final Temperature - End * °F
Expansion Factor
Calculated Acceptance Volume Gallons
Calculated Total Volume Gallons
WATTS Model Tank Volume
(Gal)
Tank
Acceptance
(Gal)
MAX. PRESSURE (PSI)
Residential Tanks
DET-5-M1 2.1 0.85 150
DET-12-M1 4.5 1.8 150
DET-20-M1 8.5 3.2 150
DET-35-M1 14.0 5.6 150
Residential Tanks
PLT-5 2.1 1.26 150
PLT-12 4.5 2.8 150
Commercial Tanks (ASME CODE)
DETA-5 3.5 1.3 150
DETA-12 5.0 3.1 150
DETA-20 8.0 3.1 150
DETA-30 15.0 10.5 150
DETA-42 22.0 15.5 150
DETA-60 26.0 15.5 150
DETA-80 35.0 15.5 150
DETA-100 45.0 21.0 150
DETA-125 60.0 21.0 150
DETA-160 70.0 52.5 150
DETA-180 80.0 52.5 150
DETA-210 90.0 52.5 150
HIDE CHART
  1. Using the calculated acceptance volume and the calculated total volume, select a tank from the chart to the right.
    • Tank volume of the selected model must be greater than the calculated total volume.
    • Tank acceptance of the selected model must be greater than the calculated acceptance volume.
    Note: Both the Tank Volume and the Acceptance Volume must be greater than the calculated volumes as indicated.
  2. A pressure reducing valve should be installed on the supply when system pressure exceeds 80psi.
  3. To accommodate the thermal expansion required for higher temperature and/or higher pressure systems, multiple tanks may be used. Please contact the factory for sizing information.
  4. For complex tank sizing for multiple apartments/condos, please contact the factory for sizing information.
  5. The potable water expansion tank shall be installed in the cold water service pipe line on the supply side of the water heater (or water storage tank).
 
     
     
     
Danger – Scalding Lurks!
Every year, thousands of people in the United States suffer serious thermal shock or scalding injuries in their bathtubs, sinks and showers.

Click here for informative resources to help you protect against these dangers.
This guide to Steam Traps explains how each style of trap functions and how to select the proper steam trap for your application. Includes application diagrams and trap cutaway views.

To learn more about Steam Traps and how they work, click here.

Canadian Customers
Careers / Investors / Terms of Use / Privacy Policy
© 2010 Watts
A Watts Water Technologies Company. All Rights Reserved.