Skip to Main Content

Naco Border Patrol Station

Watts RainCycle™ Rainwater Harvesting System Hydrates New Desert Border Patrol Facility

RainCycle-typemark

Share this Case Study

Industry

Government

Category

Rainwater Harvesting

Product(s) Installed:

Watts RainCycle™ Rainwater Harvesting System

Customer:

Naco, Arizona Border Patrol Station

 

Location:

Naco, AZ

 

Scope:

Complete sustainability for the new Naco Border Patrol Station

 

What Client Needed:

With the new Naco Border Patrol Station being based in the Chihuahuan Desert, every drop of water counts. The client wanted to enhance sustainability and conserve as much water as possible.

 

Solution:

The Naco Border Patrol Station chose a Watts RainCycle™ rainwater harvesting system.

 

Result (ROI):

The Watts RainCycle™ system has enabled them to use rainwater for irrigation and toilet flushing.

 

Summary:

In October of 2010, ground was broken for a new $40 million, 58,000 square-foot facility, the Naco Border Patrol Station. The key design criterion: sustainability. The station was equipped with a Watts RainCycle™ rainwater harvesting system because in the Chihuahuan desert, every drop of the life-giving natural resource counts.

Buried underground are two, 25,000-gallon fiberglass water storage tanks; the centerpiece of the new RainCycle™ rainwater harvesting system. The building’s standing seam roof will collect nearly half a million gallons each year. This water, which ends up in the underground tanks, will be used to irrigate outdoor plants and grass and also to flush toilets inside.

The system, like all Watts RainCycle™ systems, has four major components: inlet filtration, storage, a Rainset™ and treatment components. The self-cleaning inlet filtration is buried just below grade, with a manhole cover for access. What little sediment that collects on the filter is flushed into the system overflow. After passing through a series of strainers, the water continues into the subterranean storage tanks.

The Rainset™ is built on a skid in the mechanical room and serves as the control station, treatment station, and pressure booster pack all in one. Although there’s a submersible pump in each of the tanks, the Rainset™ at Naco includes a dual pump system with two, five-HP pumps to boost water pressure for toilets and the sprinkler system. Monitoring, pump and cleaning controls are also mounted on the skid.

Jeff Jones
Project Manager
RKS Plumbing and Mechanical Inc
Where there’s little rain, there’s all the more reason to rein-in as much of it as possible, and that’s what they’ve chosen to do.