Snow Melting Goes Mainstream in Residential Projects

 

What the Client Needed

Radiant snow melt systems are often associated with luxury properties, large custom homes, or high-end commercial projects. For many homeowners, the assumption is simple: the technology is effective, but it is cost-prohibitive and impractical for a standard residential setting.

That perception was exactly what a Mississauga, Ontario resident believed. Living in a typical 3,300-square-foot home in a suburban neighborhood, he had never seriously considered installing snow melting. Like many homeowners on his street, his driveway and walkway were finished with paving stones, and snow removal relied on traditional methods like shoveling or snow blowing.

When the homeowner decided to replace his driveway, he saw an opportunity. Still, the question remained whether a snow melt system could make sense outside of the high-end market.

Solution

The homeowner installed a radiant snow melt system using Watts 5/8” RadiantPERT pipe, paired with a Watts manifold and a tekmar Snow Melt Control 671.

The installation covered approximately 1,000 square feet across the driveway and walkway. The system runs on natural gas and is controlled to activate as needed during snowfall events, providing consistent, automated performance without manual intervention.

What makes this project noteworthy is not just the technology, but the setting. This is not a custom estate or a showcase home. It is a standard suburban property, demonstrating that snow melting can be incorporated into everyday residential applications.

Results

Despite initial concerns about operating costs, the system proved surprisingly affordable to run. The homeowner reported that his annual natural gas costs remained within a typical range, with the snow melting system itself operating at approximately $1.60 per hour during use. Even during a significant 15-inch snowfall, the system performed reliably without a major cost impact. It cleared and dried the driveway in about 23 hours for roughly $37 in energy costs, less than the price of hiring a professional snow removal service.

The perceived cost of a residential snow melting system is often higher because installation typically requires removing and repaving the existing driveway. But when a homeowner is already planning a driveway replacement, it becomes an ideal time to add snow melting. With the driveway already opened up, the remaining costs are primarily for the system components and ongoing operation.

Beyond cost, the biggest benefit has been convenience. Snow and ice melt automatically, eliminating the need for shoveling or snow blowing and improving safety on both the driveway and walkway.

The installation has also sparked interest within the neighborhood. Neighbors accustomed to traditional snow removal methods have taken notice, often expressing surprise that a system like this is both achievable and practical in a standard residential setting.


tekmar-logo-tagline

Share this Case Study

Location

Mississauga, Ontario, Canada

Industry

Residential

Category

Snow Melting

Product(s) Installed

tekmar Snow Melt Control 671, Watts manifold and PEX tubing