tekmarNet Communication
A tN4 Gateway 486 enables web browser access to heating and cooling settings from anywhere in the world. Customers can conveniently set the temperatures back while on vacation and bring their systems out of energy saving mode before arriving back home. Contractors can also take advantage of the ability to view temperature trends and make adjustments remotely. An ‘always on’ internet service is required to access the system through the internet. For customers who want to control the system from their home computer, all that is needed is an internal connection to the Gateway server. For complete details, refer to the literature tab on the product page for the most current version of the installation manual.
A tN4 Gateway 482 provides access to tekmarNet thermostat settings through a home automation system. Customers can view and adjust room temperature settings with the same remote control, touch screen or software application that controls lighting, entertainment and security settings. Drivers are available for the most popular home automation brands including AMX, Control4, Crestron, Elan, Savant, and Vantage.
tekmarNet User Switches provide one touch adjustment of the system from a wall mounted location in the home. Access away, occupied and unoccupied temperatures in all connected thermostats and setpoint controls. In a system with a tN2 House Control 400 - 403 , the away temperature setting can also suspend domestic hot water generation to save additional energy. The tN4 User Switch 480 offers customizable operation and can send a signal to a home automation system.