ArmorTek

What’s this Coating on my Valve?

Your valve has been coated with ArmorTek®, a patented, proprietary 3-part system that provides unparalleled protection against microbiologically induced corrosion (MIC). ArmorTek® has been protecting backflow preventers for years and is now standard on select ACVs/PRVs. How tough is an ArmorTek-coated ACV? We stand behind it with an 8-year MIC Warranty.

Contact a Rep

What Causes Microbiologically Induced Corrosion (MIC)?

Several factors can contribute to a corrosive environment. One of the most challenging forms of corrosion is MIC, or Microbiologically Induced Corrosion. MIC, a damaging process where microorganisms, like bacteria and fungi produce corrosive byproducts, is enemy #1. These microorganisms create biofilms on your valve’s surfaces, trapping corrosive substances and promoting localized corrosion. Over time, MIC weakens your valve, leading to leaks, poor performance, and potential failure. MIC poses a significant threat to ACVs/PRVs and backflow preventers and can compromise their reliability and functionality.


The best way to deal with MIC? Avoid it with ArmorTek®

Field-proven Protection

These images were taken in the same municipality where chlorine levels were low, and MIC activity was high.

ArmorTek

Standard Coating

In just 14 months post-install, this competitor’s valve is covered in tubercles and experiencing extensive corrosion.
ArmorTek

ArmorTek® Coating

After 16 months installed in the same municipality, this ArmorTek® valve is experiencing little to no corrosion. Limited corrosion resulting from a breach in coating is completely contained and has not spread.

Why ArmorTek®?

MIC is a leading killer of valves. ArmorTek® is a patented, triple-layer advanced coating system that helps defend against corrosion, extending the life of your ACV/PRV or backflow preventer.

ArmorTek

Primer

Electrochemical inhibitor defends iron substrate in the event of exposure from wear or impact
ArmorTek

Microbial Inhibitor

Prevents the growth of MIC and the tubercles that clog and foul equipment
ArmorTek

Topcoat

Epoxy polyester bonds to the primer forming a durable barrier

Where do Corroded Valves Go?

A corroded valve that’s filled with pinholes and fouled by tubercles can’t be repaired or recycled, which means it will end up in a landfill. Valves coated with ArmorTek® not only can be repaired, but at the end of their lifespan can be salvaged and reprocessed into new items, reducing waste and environmental impact.

ArmorTek

How it Works


Spec and buy your normal valve, it arrives with ArmorTek® coating
Install as usual
Enjoy reliable corrosion protection that will protect your valve and extend its lifespan

*ArmorTek coating is applied to select ACVs/PRVs and backflow preventers at our U.S.-based factory

Browse ArmorTek® Coated Products

Want to learn more? Need support? We’re here to help.

Fill out this form and your local rep will reach out.



By clicking submit, you agree to our Terms of Use and Privacy Policy.