Canada: T: (905) 332-4090, F: (905) 332-7068, Watts.ca
Latin America: T: (52) 81-1001-8600 | Watts.com
A Durable Drains Solution for Wolf Brewing Company
What the Client Needed
Solution
To meet these requirements, the project team, including Manufactures’ Rep Vernon Bitzer Associates and others, decided on BLÜCHER trench drains, plus a mix of other stainless steel and cast-iron Watts drains.
The BLÜCHER HygienicPro® stainless steel drains and channels were selected because their channel design evacuates waste faster than standard trench drains. They also withstand the high water temperatures during the brewing process, which can cause some products, like PVC piping, to melt, soften, and break down over time. Highly durable, they are designed to last for the lifetime of the building.
The BLÜCHER drains were also selected to help prevent failure in the surrounding flooring and related products. With its rounded edges, the HygienicPro® helps to decrease the potential for floor cracking and stress at the point where the trench, concrete, and floor coating meet.
Results (ROI)
Share this Case Study
Customer
Location
Industry
Category
Product(s) Installed:
Derek WolfCo-founder/Head BrewerWolf Brewing Company...knowing that any amount of steam, boiling water or wort, acids, caustics, or other chemicals cannot cause the drains to fail is priceless.