Granite Club Solves Long-Standing Water Temperature Issues with IntelliStation Digital Mixing Valve

 

What the Client Needed

The Granite Club in Toronto, Ontario, is a premier private social and athletic club offering members a range of amenities, including athletics, dining, and salon services. However, the club faced a persistent problem—fluctuating water temperatures in its salons and showers. Members frequently complained about inconsistent temperatures, with some even experiencing scalding water.

The root of the issue was two existing master mixing valves, which struggled to keep up with the club’s high demand for precise temperature control. One of the club’s plumbers noted that this had been a recurring problem for the 13 years he had worked there, causing ongoing frustration for both staff and members.

Solution

The Granite Club needed a solution that could meet its tight temperature control demands, which made the IntelliStation digital mixing valve the best choice. The IntelliStation delivers precise water temperature control, maintaining settings within ±2°F for consistent and reliable performance. Unlike traditional thermostatic mixing valves, which can fluctuate by up to ±7°F, the IntelliStation responds quickly to demand changes like those the of the club, preventing temperature spikes and helping to ensure a comfortable and safe water supply. Its advanced digital controls provide real-time adjustments, made it ideal for The Granite Club that required stable and accurate water temperatures.

Results

Once installed, the impact was immediate. The new system provided quick and precise temperature adjustments, eliminating the risk of scalding and improving overall comfort. “The IntelliStation is quick acting. It’s using less hot water and now using return water, which helps create big savings,” said the plumber. “The Intellistation mixes more of the return water into the cold water, adding a little of the high temperature water from storage tank so that we can maintain a 125°F supply.”

By resolving a long-standing issue, the club not only improved the experience for its members but also achieved greater efficiency in water usage.

watts-logo

Share this Case Study

Location

Toronto, Ontario

Industry

Commercial

Category

Mixing Valves

Product(s) Installed

IntelliStation Digital Mixing Valve

Granite Club Plumber

“The IntelliStation is quick acting. It’s using less hot water and now using return water, which helps create big savings”