Canada: T: (905) 332-4090, F: (905) 332-7068, Watts.ca
Latin America: T: (52) 81-1001-8600 | Watts.com
Preserving History at the Perry Belmont House with Leak Defense
What the Client Needed
Built in 1909 by Eugene Sanson, a renowned French architect, the Perry Belmont House is an architectural masterpiece and a living museum of craftsmanship. Its halls are adorned with priceless artwork, ornate vases, hand-carved stonework, and century-old hardwood floors.
However, even the most carefully maintained historic property faces modern challenges. Late one Friday night, as the caretaker was packing up to leave for the weekend, he heard the sound of running water. A pipe had burst inside the mansion, and as he searched for the source, he eventually entered the room with the hand-painted ceiling mural. By sheer luck, he caught it in time — otherwise, the incredible “Easter Stars” mural and several other priceless paintings could have been lost. After this, the property manager knew that relying solely on periodic inspections and luck was no longer enough. Another leak could mean permanent loss.
Solution
To prevent future water damage and gain peace of mind, the property manager turned to Leak Defense. Designed to detect and stop leaks before they cause damage, the system provides continuous protection across the property. Leak Defense technology monitors water flow in real time, instantly shutting off the water supply and sending users a notification when irregular activity is detected — whether it’s a slow drip behind a wall or a burst pipe in a remote section of the building.
Results
Installation was completed without compromising the integrity or aesthetics of the historic home. Now, the Perry Belmont House has modern protection working quietly behind the scenes, safeguarding the property from the threat of water damage 24/7.
Share this Case Study
Location
Washington D.C.
Industry
Commercial
Category
Leak Detection
Product(s) Installed
The Leak Defense System