Watts Drains Meet High‑Rainfall Demands on a Multifamily Roof System

 

What the Client Needed

The Prose multifamily apartment complex in Houston, Texas, consisting of 314 units and targeting completion in January 2027, required a roof drainage and exterior water‑sourcing system capable of withstanding the region’s intense rainfall patterns. The project team needed an approach that would provide both primary and backup drainage to protect the buildings’ long‑term performance, as well as freeze protection for exterior water access. To keep construction on schedule, the contractor and wholesaler also needed rapid local product availability, consistent quality, and strong technical support.

Solution

Watts roof drains and roof hydrants were selected as the most reliable solution for meeting the project’s performance standards. The RD‑300 series roof drains were chosen for their ability to manage high‑volume drainage, and the 2‑inch external water dam option added essential backup protection to the primary drainage system to maintain roof performance during extreme rain events. For exterior water access, the HY‑900 roof hydrant was installed because it automatically drains when shut off, reducing the risk of freezing and preventing potential damage to both the hydrant and the piping system.

Results

The project’s success strengthened the ongoing relationship among the partners involved, resulting in the continued use of Watts products for several additional multifamily developments across the Houston area in 2025. What began as a single project requirement evolved into a long‑term collaboration built on trust, performance, and a shared commitment to high‑quality construction.

watts-logo

Share this Case Study

 

Location

Houston, Texas 

Industry

Multi-family

Category

Drainage

Product(s) Installed

Watts RD-300 Roof Drain & HY-900 Roof Hydrant