The Cooling Challenge AI Data Centers Can’t Solve With Capacity Alone
Key Takeaways
- AI data centers need engineered thermal storage in technical cooling loops where short-duration rack demand can outpace upstream cooling response.
- High-density AI racks can create fast thermal spikes that last seconds or minutes but still affect rack performance.
- Added chiller capacity or longer piping runs may increase system volume without preserving usable chilled water temperature near the load.
- Stainless steel thermal energy storage (TES) tanks can help maintain supply-water stability by improving how stored water behaves during transient demand events.
- Early design evaluation can help architects, engineers, and owner/operators reduce rack performance risk, rework, commissioning delays, and unnecessary strain on chillers.
For years, data center cooling systems were engineered around more predictable IT loads and steadier operating profiles. Capacity planning, redundancy targets, and equipment sizing gave design teams a dependable framework for maintaining performance. Initial AI model training followed the same pattern, just at higher cooling demand levels.
However, agentic AI is changing data center cooling design by creating faster, denser, and more volatile rack-level thermal demand than many traditional cooling strategies were built to manage. As AI infrastructure continues to compress more heat load into smaller footprints, the load profile is shifting from predictable demand to larger, less consistent swings that can challenge cooling response at the rack.
The most challenging thermal impact events may last only 30 seconds to a minute, but that can be long enough to affect rack performance. When the thermal event occurs inside the technical space, useful cooling needs to be available close enough to stabilize the loop before upstream equipment catches up. That timing gap is what turns AI cooling from a capacity-sizing exercise into a resilience design problem.
How Is AI Changing Data Center Cooling Design?
For years, data center cooling systems were engineered around more predictable IT loads and steadier operating profiles. Capacity planning, redundancy targets, and equipment sizing gave design teams a dependable framework for maintaining performance. Initial AI model training followed the same pattern, just at higher cooling demand levels.
However, agentic AI is changing data center cooling design by creating faster, denser, and more volatile rack-level thermal demand than many traditional cooling strategies were built to manage. As AI infrastructure continues to compress more heat load into smaller footprints, the load profile is shifting from predictable demand to larger, less consistent swings that can challenge cooling response at the rack.
The most challenging thermal impact events may last only 30 seconds to a minute, but that can be long enough to affect rack performance. When the thermal event occurs inside the technical space, useful cooling needs to be available close enough to stabilize the loop before upstream equipment catches up. That timing gap is what turns AI cooling from a capacity-sizing exercise into a resilience design problem.
Can Today’s Cooling Strategies Support AI Rack Loads?
Today’s cooling strategies can support AI rack loads only when they account for how quickly rack density, power demand, and thermal behavior are changing. Hardware density is advancing faster than many data center projects can move from concept to commissioning, which means a rack configuration selected during design can be overtaken by newer hardware, higher power densities, and different demand profiles before the facility reaches full operation.
That pace compresses a planning cycle that used to unfold over five to ten years into just 18 to 24 months. For architects, design engineers, and owner/operators, the cooling system must account for a moving target: long construction timelines on one side, rapidly changing AI rack requirements on the other.
The trajectory is already visible. In 2021, typical rack power ranged from 25 to 30 kW. By 2024, power had doubled to roughly 60 kW. Just one year later, rack power doubled yet again to approximately 120 kW. Experts expect this trend to continue, suggesting rack powers as high as 200 kW by the end of 2026 with future designs scaling higher still.
Why Doesn’t More Cooling Capacity Automatically Create More Resilience?
More cooling capacity does not automatically create more resilience because rack-level thermal events can occur faster than controls, hydraulics, pumps, and chillers can adjust. A central plant may be sized for expected peak demand and still leave the technical loop exposed during rapid short-duration spikes.
Additional chillers, larger distribution infrastructure, or broader redundancy may be necessary for some projects, but those investments cannot by themselves resolve the timing gap between heat generation at the rack and cooling response from the plant. A facility can look properly sized on paper while still experiencing short-term temperature excursions where AI loads are concentrated.
Designs built tightly to specification are especially vulnerable. Buffer and redundancy are expensive, space is limited, and teams are under pressure to maximize compute density. When rack configurations shift or demand behaves differently than expected, resilience depends on where usable cooling is available, how quickly it can be applied, and how effectively the loop maintains temperature during transient events.
How Does Thermal Storage Help Cooling Systems Handle Rack-Level Heat Spikes?
Thermal storage helps cooling systems handle rack-level heat spikes by adding usable thermal inertia at the point of demand. During a short demand spike, localized storage can absorb part of the thermal load and help preserve stable supply-water conditions near the rack while chillers, pumps, valves, and controls adjust to the increased cooling demand.
That ride-through capacity changes how the cooling system experiences AI-driven volatility. Rather than requiring the entire plant to follow every rapid rack-level load change immediately, thermal storage can smooth the event before it propagates through the system. In high-density AI zones, this helps maintain the technical loop during the brief window between a GPU-driven heat spike and full upstream cooling response.
Stainless steel TES tanks add another layer of value by making that storage more controlled and usable. In this application, the engineering of the tank determines how effectively stored cooling can be used. Flow management and temperature stratification can help reduce the risk that return-water movement quickly compromises the available chilled-water reserve.
Why Should TES Tanks Be Evaluated in the Technical Cooling Loop?
TES tanks should be evaluated in the technical cooling loop because AI cooling volatility is occurring closest to the rack. Storage located farther upstream may still support plant-level performance, but technical-loop storage can provide ride-through value where rapid demand changes are most likely to affect rack conditions.
Placed in the technical loop, a stainless steel TES tank can add localized thermal inertia where the volatility is occurring. During a short AI-driven demand spike, that reserve can help maintain water temperature longer, reduce the immediate load on chillers, and create smoother operating conditions for the broader plant.
This is also where the design conversation becomes more difficult. Technical spaces are valuable, and teams may hesitate to place water storage in clean-side or rack-adjacent environments. Cost, footprint, service access, and leakage concerns all deserve careful evaluation before the cooling architecture has already been locked in.
For owner and operators focused on uptime and risk management, the decision is about determining whether the technical loop has enough controlled thermal inertia to protect increasingly dense AI loads while reducing the strain that short-duration peaks place on upstream equipment. A stainless steel, single-pressure-vessel TES tank can help make the conversation more practical. The design can provide engineered storage without introducing the same profile of complexity associated with some distributed or multi-component approaches.
What Happens When AI Cooling Volatility Is Ignored?
Ignoring AI cooling volatility can lead to rack performance degradation, system rework, commissioning delays, added labor burden, and avoidable pressure on the cooling plant. These risks become more likely when the system is designed around steady-state capacity but lacks enough ride-through capability for fast demand spikes.
In AI environments where high-value compute is packed into dense footprints, brief instability can carry meaningful consequences. If supply-water temperature cannot remain stable during a short thermal event, performance can degrade even when the installed cooling capacity appears adequate.
The project risk can be just as significant. If cooling volatility is discovered late, teams may need to revisit piping layouts, add equipment, adjust controls, or redesign portions of the system during construction or commissioning. Those changes can add labor, delay schedules, and create avoidable coordination issues across engineering, construction, and operations teams.
When Should Data Center Teams Consider TES Tanks in the Design Process?
Data center teams should consider TES tanks early in the design process, before space planning, loop architecture, and cooling criteria become difficult to change. The evaluation should begin when teams are identifying high-density AI zones, expected rack trajectories, transient load behavior, and technical-loop performance requirements.
Early evaluation does not mean every project needs the same storage strategy. It means architects, engineers, and owner/operators should ask whether the cooling system has enough localized thermal inertia to handle realistic AI demand volatility. That question belongs alongside capacity, redundancy, controls, serviceability, leak detection, access, and lifecycle cost.
The strongest designs will likely come from treating TES tanks as a system-level resilience option rather than a late-stage add-on. When the conversation happens early, teams have more flexibility to allocate space, evaluate technical-loop placement, coordinate monitoring and leak detection, and determine whether stainless steel thermal storage can reduce risk more efficiently than expanding the entire plant.
How Should AI Data Centers Design for Cooling Resilience?
AI data centers should design for cooling resilience by pairing capacity planning with localized ride-through strategies in the loops most exposed to transient rack demand. In high-density AI environments, cooling performance depends on how effectively the system uses installed capacity during the short window between a demand spike and the full plant response.
That shift places engineered thermal storage closer to the center of the design conversation. Stainless steel TES tanks can help preserve chilled-water stability, reduce chiller strain, and protect rack performance during short-duration demand spikes that traditional capacity planning may not fully address. Their value is strongest where AI rack density, fast load changes, technical-loop constraints, and tight design margins converge.
As AI continues to reshape data center infrastructure, the most resilient facilities will be the ones that identify where thermal volatility exists and design controlled thermal inertia into the system before the risk appears in operation. For many high-density AI projects, that means evaluating stainless steel TES tanks in the technical cooling loop as an early design decision, not a retrofit conversation after rack demand has already outpaced the original design basis.
About the Author
|
|
Greg Berry Director of Sales, CoolVault™ Thermal Energy Storage Solutions Bringing more than 25 years of experience in sales, business development, and technology solutions for industrial and enterprise customers, Greg Berry works with customers, engineering firms, and strategic partners to improve cooling efficiency, operational resiliency, and sustainability. ludes leadership roles at Watts, Carrier, and Philips, and he holds a Bachelor of Science in Electrical Engineering Technology from Purdue University. |