In AI Data Centers, Just Detecting Leaks Is Not Enough

AdobeStock_2021030088 (1)

Key Takeaways

  • AI workloads are accelerating liquid cooling adoption, placing water closer to the systems that support uptime and compute performance.
  • As water moves closer to critical equipment, the impact of a leak can outweigh the likelihood of the leak itself.
  • Many traditional leak protection systems stop at detection, leaving operators to interpret alarms, locate valves, and decide how to respond under pressure.
  • Stronger leak protection starts with preplanned thresholds: how much water can escape, which assets are exposed, and when the system should alert, isolate, or shut off flow.
  • Data center designers, specifiers, engineers, and operators should treat leak response as a design decision built into every applicable cooling-water loop.

 

Before the advent of AI, data centers treated water near critical IT and electrical infrastructure as a risk to be managed, minimized, and isolated. That philosophy shaped facility design for decades. Leak detection systems provided early warning and facility teams responded reactively as alarms occurred. Generally, the model worked because water played a relatively limited role inside the computing environment itself. Now, however, as AI workloads drive unprecedented increases in rack density and thermal output, the way data centers use water is rapidly changing. As liquid cooling systems bring water closer to the capital equipment that sustains compute performance, every leak carries greater operational risk. Early detection and proactive risk management have become essential to protecting cooling availability, uptime, equipment, and continuity before a localized failure has time to spread.

Why is Liquid Cooling So Important in Data Centers?

Liquid cooling is no longer optional in data center design because AI workloads are pushing rack densities beyond what many traditional air-cooling strategies can efficiently manage. AFCOM’s 2026 State of the Data Center report found average rack density jumped from 16 kW to 27 kW per rack, rising nearly 70% in one year, while 69% of respondents expect rack density to increase further over the next 12 to 36 months. Some experts project total AI data center capacity demand will increase 3.5 times by 2030.

That growth is changing how facilities approach cooling systems and the fluid infrastructure engineered to support them. As water moves closer to high-density compute infrastructure, leak detection becomes a non-negotiable frontline safeguard against mechanical failures that can threaten cooling availability, uptime, and equipment safety.

Table detailing methods of data center cooling, typical capacity, operational complexity, and future AI sustainability

Why Isn’t Leak Detection Alone Enough for AI Data Centers?

Many traditional leak protection systems stop at detection. They alert personnel to discharging water but rely on manual intervention to manage the consequences. In denser, more water-dependent facilities, the delay between alarm and action can be the difference between a momentary maintenance headache and half-a-million dollars in unplanned downtime.

Many facilities still rely heavily on rope-style leak detection systems placed near vulnerable equipment. These systems can identify the presence of water, but they do not determine severity, isolate affected piping, protect nearby assets, or decide whether the right response is observation, escalation, local shutdown, or automatic intervention.

The reality is that detection alone does not manage consequences. Water typically does not behave in predictable ways after a failure. It can travel far beyond the origin of the leak, particularly in large colocation environments and facilities with extensive piping infrastructure.

A sensor may confirm that water exists, but it cannot determine whether the event threatens critical power infrastructure, server operations, or personnel safety. A stronger leak protection strategy answers these operational questions before the alarm occurs.

Why Should I Invest in Stronger Leak Protection?

In the case of AI data centers, the potential economic impacts of just one leak warrant proactive investment. According to Uptime Institute's 2025 outage analysis, more than half of respondents reported outage costs exceeding $100,000, while one in five reported costs greater than $1 million. Human error also remains a significant contributor to outage events.

The data center industry has long accepted that low-frequency events can still justify significant investment when the consequences are severe. Backup generators, redundant power systems, fire suppression infrastructure, and disaster recovery strategies all exist because organizations recognize that the impact of failure matters as much as the likelihood of occurrence. Leak protection should be viewed through the same lens.

The most effective strategies begin by defining acceptable levels of risk before a facility becomes operational. This avoids relying on the unpredictable behavior of an individual under stress and turns leak response into a planned sequence of decisions the system and staff are prepared to execute.

 

  • How much water can safely escape in each area?
  • Which assets are exposed?
  • At what threshold should alerts, isolation actions, or automatic shutdown occur?

 

When those decisions are made during design rather than during an emergency, response becomes faster, more consistent, and less dependent on individual judgment. Risk is reduced because operators are not starting from a blank slate: they have defined thresholds, trained staff, known response steps, and isolation logic that can limit the radius of failure before water reaches critical equipment.

That planning should also be treated as a living process. Annual evaluations, staff training refreshers, post-event reviews, and feedback from maintenance teams can reveal whether response logic still matches the facility’s risk profile, especially as cooling systems expand, rack densities increase, or equipment layouts change.

Real-World Data Center Leaks & Their Impacts

No single incident should define an industry's design philosophy. However, several public incidents illustrate an important reality: a leak that begins as a mechanical issue can quickly become an electrical issue, an operational issue, a safety issue, or a business continuity issue.

 

 

Together, these incidents show why leak protection cannot end at awareness. Once water escapes containment, the question becomes how quickly the facility can limit the radius of failure, isolate the affected loop, and keep a localized failure from turning into a broader operational event.

How Can Data Centers Improve their Response to Leaks?

Data centers can improve leak response by treating detection as the trigger for a preplanned action, not merely as an alarm. In high-density facilities, the system should already know when to notify operators, when to isolate a loop, and when to shut off flow before water reaches critical equipment.

The design question is not simply, “Did the system detect water?” It is, “Did the system respond in proportion to the amount of water, the rate of release, and the equipment at risk?” That shift requires teams to decide the price-risk tradeoff early in the project. If a facility determines that a certain volume of escaped water is unacceptable in each area, the leak protection strategy should translate that threshold into programmed response logic for the water mechanical cooling system.

This also prevents overreaction. A nuisance event should not shut down an entire data center, but stopping a high-flow release should not depend on someone finding the right valve under emergency conditions.

For data center designers, specifiers, MEPs, and architects, the next step is clear: build response logic into every applicable loop in the cooling-water system. Define thresholds, isolate risk locally where possible, and give operators clear visibility into what happened, where it happened, and what action the system has already taken.

Conclusion

AI-driven data center growth is forcing the industry to rethink a range of long-standing assumptions about power, cooling, density, and resilience. Critical to this evolving understanding of fluid infrastructure is rethinking how water risk is handled.

Facilities need a more mature approach to resilience, one that considers not only how leaks are detected, but how their consequences are contained.

Now is the time for data center designers, specifiers, engineers, and operators to evaluate whether their leak-protection strategies stop at detection or extend through containment and automated response. Review cooling-water loops, response thresholds, isolation capabilities, and operational procedures. Build intervention logic into the design process to determine whether today's protection strategy is aligned with tomorrow's risk profile.

 


About the Author

Keith Zander HeadshotKeith Zander
Senior Product Manager, Commercial Applications & Solutions
Leak Defense, A Watts® Brand
 
Keith Zander has decades of experience in the application of elegant solutions to complex problems in the energy and sustainability market. His experience ranges from renewable energy, data center climate control, emergency power systems, HVAC for light aircraft, heavy truck & offroad equipment. In his current role, he enjoys working with all the influencers in developing and applying cost-effective solutions for protecting all types of structures against the financial perils of catastrophic water damage.