Canada: T: (905) 332-4090, F: (905) 332-7068, Watts.ca
Latin America: T: (52) 81-1001-8600 | Watts.com
The Big House in York
Share this Case Study
Industry
Single Family Housing
Category
Product(s) Installed:
Customer
Bob Myers
Location
York, PA
Scope
Quality mechanical systems using radiant heat for a new 8,500 s.f. home, with an additional 4,000 s.f. of living space below ground.
A highly efficient system that would cost effectively provide heat and hot water for the family’s new home
Installer
Dave Yates, President, F.W. Behler, Inc.
Solution
14,000 s.f. of Watts SubRay above-subfloor panels, plus three Watts home-run domestic water manifolds and fed by WaterPEX tubing and two inches of rigid insulation under the entire home, and its perimeter.
Result (ROI)
Even with ambient temperatures at zero degrees one year, the homeowners were able to warm the entire home with first- and second-floor temperatures of 88°F.
Dave YatesPresidentF.W. Behler, Inc."This radiant heat solution puts BTUs close to the finished floor surface, so we were able to reduce system delivery temperatures dramatically."