Canada: T: (905) 332-4090, F: (905) 332-7068, Watts.ca
Latin America: T: (52) 81-1001-8600 | Watts.com
Homeowner Seeks to Provide Safe Drinking Water for Newborn
What the Customer Needed
A homeowner in Mississauga, Ontario, Canada was in search of a reliable, affordable water filtration system for his family. As a child, he grew up near a water treatment plant which resulted in poor water quality. Because of this, he developed spots on his teeth which his dentist attributed to this. With the birth of his child, the homeowner wanted to ensure his son will always have access to clean and quality drinking water.
Solution
The homeowner’s neighbor recommended the Watts PWDWHCL1 Single-Stage Lead Filtration System, which he had installed previously. The PWDWHCL1 is a 2 GPM under counter high-capacity water filtration system certified to remove 99.2 percent of lead from water. This high flow system also reduces cysts, chlorine, odor, sand, silt, dirt and rust for safer, better tasting water.
The homeowner went beyond the traditional under counter installation because he wanted to hook the system up to the refrigerator line as well. “Installation was super easy, there were no issues” he said.
Results (ROI)
Since the Watts PWDWHCL1 Single-Stage Lead Filtration System has been installed, the family has been able to enjoy clean, better tasting water without the concern of contaminates. “It’s great to have confidence that we are drinking clean, filtered water,” the homeowner said.
Share this Case Study
Customer
Location
Industry
Category
Product Installed:
HomeownerIt’s great to have confidence that we are drinking clean, filtered water.